Hello,
i have biuld a circuit with a PGA 2311 and he is to qiet. It is louder when i bridge the input pins to the output pins. Its louder without the PGA2311. I have used the recommended Connection from the PDF (Figure5). At start N is 150 and i didn't hear anything out of the speakers and if N is 255 i can hear the sound, but it's not as loud as i can hear without the PGA2311. The power supply is VA+ 5,1V , VA- -4,9V and VD+ 4,97V. The transformer for the Analog side has 1,8VA and 2x6V. 7805 and 7905 regulate the Voltage.
I hope you can help me.
Marius