Hi,
There is mentioned in the data sheet about the I2S serial output as below.
Is the I2S serial output fixed 48kHz if using MCLK : 12.288MHz(fixed), the input sampling rate : from 32kHz to 48kHz ?
if the I2S serial output is fixed 48kHz without depending on it, how does TAS5548/58 realize this feature ?
Could you please tell us the internal topology in detail ?
Bestregards,
Kato