Hi. I'm just hoping for some pointers for attaching a PCB with a DKD package to a heatsink. SLMA004 mentioned in the TAS5630DKD data sheet doesn't have any relevant information regarding the package where the heat slug is on top. The top of the package has a tolerance of 0.5mm. If I'm going to be sure of good thermal contact in the worst case it means the PCB could be bent 0.5mm if the package is at the high side of the tolerance. The amount of pressure on the slug is determined largely by the thickness of the board and distance of the mounting points from the chip but I can't find any mounting guidelines at all.
tia
Gordon