Hello
My customer had chosen TPA3251D2 for next year model because TPA3251 has very low THD and High bandwidth.
Here I had 3 questions from customer below.
Q1 I don't kno slave mode1, slave mode2 well.
What is the usage / purpose of the slave mode 1 and slave mode 2 ?
Does it change the order of inter_channel_delay for each half bridge?
Please refer attached.
Q2 When IC1 is master. How do I do for IC2 and IC3 for slave?
IC2 and IC3 should be same slave mode 1?
Q3 Please advise your recommended setting for wide bandwith 40KHz +/- 1dB
I intend to suggest 10uH/0.33uF to customer,,,,
Best Regards