Is it possible to seperate the digital signal to low frequency and high frequency band inside TAS5766 before sending to the low-frequency speaker and high-frequency speaker?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is it possible to seperate the digital signal to low frequency and high frequency band inside TAS5766 before sending to the low-frequency speaker and high-frequency speaker?
Thanks for your help.
we are using TAS5766 Smart Amp in 1.1 Bi-Amp mode (mono) in which one output drives the Subwoofer, while the other drives the mid-range ! We hope to set the crossover at around 400Hz-500Hz, but the woofer is not completely rolloff until ~2kHz. So we also need a LP for the woofer... Is it also can be done by the passive cross-over? The woofer and the fullband speaker is in the same cabinet.
We expect to be able to do digital cross-over, likely equalization for both speakers, and take advantage of SmartAmp feature to boost up bass (TS modeling, excursion, ect)
Also want to confirm with you, if the DSP(like Smart Base, SmartEQ, SOA etc) inside the TAS5766 applies to the left and right channel together if with only one TAS5766M?
Thanks in advance.
Hi,
We are looking into integrating support for 1.1 in PurePath Console 3. Please get in touch with your local sales rep. We might have a temporary solution available while it is being implemented in PPC3.
Regards,
J-
Team-
I have a customer interested in 1.1 operation as well, but driving a mid-range and a tweeter with a single '5766.
Please let me know what the interim solution is, or otherwise send me your contact info internally so we can continue this development.
Best, S. Dunbar, AFA Colorado
Team-
A response would be greatly appreciated; I have already elevated with Don D.- please contact me internally as soon as possible.
Best, S. Dunbar, AFA Colorado
Hello
Any news on this? I have similar configuration and same problem
Regards
Jonas Svendsen
They are working on this configuration, just not sure when the tool update will be released.
Hi Ti experts,
Is there any progress of this? when will this feature be released in the PPC3?
Thx