Customer study using same DSP (BD mode) input to TAS5612LA, then switch to TAS5342LA with the same DSP PWM output, the level is lower by 7dB.
Both TAS5612LA and TAS5342LA are used in BTL mode.
DSP (BD mode) + TAS5612LA (BD mode)
Same DSP (BD mode) + TAS5342LA( AD mode - Hardware setting[m2,m1,m0- 000] ) : Output level lower by 7dB (at 1kHz).
Both frequency response are same across 20~20kHz except level different by 7dB.
Output filter
TAS5612LA(BD mode) : L=10uH, Cg=0.47uF
TAS5342LA(AD mode) : L=10uH, Cg=0.47uF , CBTL = Nil
I had checked both circuitry, except CBTL not connected in TAS5342LA, others are OK.
Question:
1) Will the mismatch of output filter cause the output level different?
2) What is the other possible causes that will result in the output level different?
3) What will happen to output if DSP (BD mode) is connected to Damp+Filter (AD mode)?
Thanks.
Best regards,
Chin