What happens when TAS5611A is driven to it's extends and at some frequencies the load impedance drops below 3 Ohms while no Schottky diodes are present from OUT_x to GND?
Can the chip be damaged? Will overload occur?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
While using the TAS5611A with filter damping RC (zobel) and schottky diodes direct to the OUT_A,B,C,D and stable constant 30V DC supply voltage the output shuts down for about 50ms while playing drum pulses in speaker load of about 3.4Ohms Rdc (PBTL, 22uH & 1uF LC filter). The ready signal goes low and the output tends to zero for these event. An overload case is not present because the /SD and /OTW flags stay high.
My feeling is the dynamic load introduces local thermal heating the TAS5611 is not capable of spreading to the heatsink...
Would it be helpful (without changing circuit parameters) to use TAS5613A or TAS5630B to get rid of this effect? Remeber the output MOSFETs may be the same with Rdson 60mOhm (typ.).
Kind regards
If you are experiencing a thermal issue, the TAS5613A or TAS5630B shouldn’t offer too much of an improvement.
Do you have a schematic you can share?
Do you have impedance plots of the load?
Have you tried to measure if schottky diodes are in fact conducting?
You may want to remove the schotty diodes as a control and see if you are experience the same issue. It may also be beneficial to check the temperatures with a thermocouple. Does the heatsink/amplifier get hot before you experience the shutdown issue?
Measuring the peak current and voltage that triggers the shutdown event may also help pinpoint the issue.
Best Regards,
Matt
We are quite sure it is a thermal effect because it is independent of schottky diodes present at the outputs or a RC network for LC-filter dampening. Removing these things doesn't change a bit while it makes difference how long the amp is on an heating itself. When TAS5611 is cold, the error won't happen while after a minute of full power output the density of drop outs increase. We also changed the thermal interface material and the pressure and found a drop dependence.
(What makes me wonder the ready flag is changing for the moment the drop out appears while the SD and OTW signals are stable...? It cannot be overcurrent with Roc=22k and +30VDC supply)
I know about the tolerances you propose for the TAS series amps. I think about changing the TAS5611APHD to TAS5613A-DKD with bigger package and better heat slug, because it is easier to bring up to the heatsink. Hope this will give better results...
BTW: the amp is working in PBTL mode. Do you know if there are issues in contrast to normal BTL?
Kind regards
Hi, assembled back to suggested values Lout=10uH, bigger coils and fsw=400kHz, but no success.
Then I have made some measurements on TAS5611A when driven into clipping with speaker loaded (woofer Rcd=3.2Ohm 6inch vented cabin). This can be seen on the first picture. Interesting to see when TAS5611A is in clipping, the switching frequency drops down from 400kHz to 130kHz.
The second picture shows the output voltage at the speaker after the amp was overdriven (some millisecond ago...). At the end of the diagram the dark blue curve shows a spike in the curve at zero crossing. Right there the dark green curve shows the BST voltage (bootstrap) where you see the output voltage and the gate drive same time. Shortly after that spike the amp stops switching (READY pin goes low for about 50ms). It restarts then, but a drop out can easily be heard.
The lower part of the diagram shows a zoom of the BST voltage (time slice when spike on output voltage accurs) where an abnormal switching behavoir takes place: the low phase of the PWM is disturbed by small pulses! And 300us later the drop out occurs.
Interesting to notice, when the max overdrive level is reduced (smaller amp input voltage) or the supply voltage is increased by 3V (more headroom) the drop outs will no longer happen!
This leads to stringend input level limitation, doesn't it? Interested in your opinion...
Hi Matthew, let me summarise the circuit: TAS5611A with 33VDC in PBTL mode, 10uH output inductors and Schottky diodes direct to the OUT_x pin, gate drive buffered locally 3R3&100nF and power inputs decoupled with four 2uF MLCCs (distance 1.5mm). Increasing the Isat of the output inductors didn't give any cure. A 3.2 Ohm speaker chassis is the target load and connected in a vented cabinet for all my measurements. I promise to you it will be interesting...
Here you see the output voltage of one summing point (speaker plus) in blue. The green curve shows the output current. You can see voltage and current are not in phase when the drop occurs:
The next picture shows the output voltage of out H-bridge output and the current throught one inductor in the moment the drop takes place (bottom=zoom):
You can see the output ripple current of 2A(pp) and the means value tends to zero...
For the moment the drop comes in here is the OUT_A and OUT_C and it's zoom and further zoom (bottom). Failing pulses takes place:
Then a little bit more to the point of interest:
In the zoom you can see the outputs, connected via two inductors to one capacitor, begin to switch against each other in a more dramatic way, phase shifted.
But now here is something new! I got a mains fail detection circuit (diode clamp, RC filtered) connected to the secondary side of the switchmode power supply. In the case of mucis pulses in conjunction with real speaker load and heavy voice coil excursion the speaker is feeding back it's energy to the power supply (known as bus pumpimg). The TAS5611A like all H-bridges can't avoid this. The designer himself has to take care of this effect. So the power supply receives current from the speaker back and because it is a system with a feedback, the supply skips PWM pulses (a lot) to avoid overvoltage at the power voltage node. Here you can see the output voltage of the mains-fail circuit (green curve) one millisecond before the drop rushes in:
That voltage goes near zero for about 2ms and so the system does what it should in case of mains-fail: The /RESET of TAS5611A is asserted and the TAS goes to reset state while signal is still present. This is the drop out and the long search of something really stupid simple signal.
The reset causes the TAS56 to finally stop for a while and the overvoltage of the supply is no longer present so the mains-fail signal rises again and the TAS-Reset is set to inactive (high). Music will be played on...
There is one thing wondering me why the TAS56xx does not stop switching at the outputs OUT_A,B,C,D and is drifting into chaotic behavior when /RESET is asserted?
After re-dimensioning the clamp circuit the amplifier now works perfect and I would like to thank you for your help and I am really sorry for wasting your time. But maybe it was interesting to you, too... ;-)