Hi There
We are considering using a LM4990 as a driver. The signal it is driving is 1 kHz sine wave with stepped amplitudes (IRIG) which is generated by a DAC.
From my reading of the data sheet, the AMP can drive about 4Vpp which is OK.
Unloaded, we would prefer slightly more (4.5V unloaded) and a minimum of 3V @ 50 ohm.
The load is isolated by a 100mH 1:1 transformer.
Does this sound feasible? Am I reading the datasheet correctly??