Hello all,
I am in need of help deciding what would be a good inductor to use for the TPA2013D1. I was going to use the recommended inductor (Sumida CDRH5D28NP-6R2NC), but it is to tall. I have a limit of 2mm, the Sumida is 2.8mm. I did find a couple inductors that look like they would fit the bill, but i'm not really sure if they would be good options.
Specs for what I have;
- Li-ion battery - 3.6V
- 4Ω speaker
- only need 2W max output power.
Here are the 2 inductors I found that I thought they would be OK.
- http://products.sumida.com/products/pdf/CDRH5D16.pdf
- http://www.cooperindustries.com/content/dam/public/bussmann/Electronics/Resources/product-datasheets/Bus_Elx_DS_4086_MPI4040.pdf
I am open to ideas for better options.
Thanks
Anthony