Dear Support,
I already wrote a post on the audio converter forum here, but the problem involves mostly the TPA3110D2, so I would post my question here.
In my two boards system I have an AM3352 CPU, a AIC3254 codec which drives the TPA3110D2 r with PBTL Output and Single-Ended Input. In the audio converter forum you can see the schematics (R in the PBTL input now is 100K).
The problem is that when I start a playback, the amplifier emits a loud click. The problem is caused by the difference of bias between the line output of audio codec (800mv) and the input of the amplifier (about 3V). When the codec output is connected a negative DC step produces a very annoying click at best, a DC fault (recoverable only by a power cycle) at worst.
What is the correct strategy to avoid this issue?
Thank you.
mario