When are we (end users) going to be able to purchase it? Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jay,
Thanks for your interest in TPA3255. The current schedule is late July/ early August. What application you're planning to use TPA3255?
Thanks Jay!
TPA3251 and TPA3255 are pin to pin compatible, so you can use TPA3251 for now and swap it out with TPA3255 when it's released. If you're designing a board be sure to design for the high voltage capability for TPA3255, which will work of TPA3255. 100V caps for PVDD and the outputs.
Hello Thorsten,
We are on schedule with the TPA3255 release. It should be released before the end of this month as planned.
Damian,
I have a question about the TPA3255 OSC_IOM & OSC_IOP pins.
I presume that if I tie the FREQ_ADJ pin to DVDD (3.3V), then the OSC_IOM & OSC_IOP pins become a differential clock input to the TPA3255.
I plan on feeding a 24.576/40=614.4kHz differential clock into these two pins.
The TPA3255 datasheet does not have much information on the specs of said differential clock.
Would you have any specs on this differential clock (OSC_IOM / OSC_IOP)?
Thanks,
Sam