Hi.
I've designed a board using an LM48511 as speaker amplifier. Sometimes, if input signal is high enough or I try increasing amplifier gain "too much", output to speaker gets to 0. Moreover, output remains low until power supply board is switched off-on. The output stage seems to get locked low and being freezed in that state.
I've found a previous post (e2e.ti.com/.../193746 ) talking of a similar problem, and explaining everything with an undervoltage on power supply VDD (below 3V). I've checked 5V VDD and it actually goes below 3V when output lock happens. I've disabled boost converter (using 5V VDD to directly supply internal opamp and output stage), but output lock still happens, eventhough less often.
What I don't understand is why output remains low even after VDD returns to nominal value 5V. Could reset signals be used to make amplifier still working without resetting power supply?
Thanks...