I think below points is typo for TAS5754M datasheet.
Please let me comfirm below.
------------------------------------
①Page-1
・The correct is HTSSOP package and 12.50mm, right?
②Page-36
・The correct is MCLK and SCLK, right?
③Page-51
・The correct is -103dB, right?
④Page-52
・Datasheet page-74 is "reserved", which is correct?
⑤Page-62
Register Map is differ from Detailed description below, which is correct?
・P0-P34(Page-70) is assigned [1:0].
・P0-P37(Page-71~72) is assigned 0bit~6bit.
・P0-P42(Page-72) is assigned [5:4].
・P0-P42(Page-72) default setting is "00000001".
・P0-P43(Page-73) is assigned [5:0].
⑥Page-67
・Are "000" and "001" both the same clock(MCLK)?
Or, is it typo?
------------------------------------
Best regards,
Satoshi