Hi team,
Can TAS5754 support using BCLK(No MCLK) 3-Wire mode at 96K or higher sampling rate?how to configure the device?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, Bing,
Yes, the TAS5754M can work in 3-wire operation mode. You need only to configure the amplifier to ignore MCLK detection since there won't be any MCLK, and set the PLL clock source as SCLK. The device will auto generate the clock coefficients. The following code showcases the required register configuration:
# Ignore MCLK and MCLK halt detection
w 98 25 18
# Set SCLK as the input of the PLL
w 98 0D 10
Best Regards,
-Diego Meléndez López
Audio Applications Engineer