My application uses two TAS5751 chips - one in PBTL mode to drive a 4-ohm woofer and the other to drive a 6-ohm tweeter.
So for the tweeter amplifier, I really only need one channel. So, in the interest of saving some power, parts and PCB area is it
allowable to:
1) Make no connection to the outputs of the unused amplifier output pins (OUT_C, OUT_D, BSTRP_C, BSTRP_D)
2) Connect but omit bypassing of the 2 PVDD pins powering the unused amplifier
I plan to use the PWM Shutdown Group Register, 0x19 to keep the unused C-D channel off and not switching.
HAL