I testing the TPA3136D2EVM connected to TI 3204 codec EVM. The amplifier is PBTL mode (J13 disengaged) and connected to the CODEC through single ended connection.
CODEC output > 1k+4.7nF filter > 1uF decoupling cap > amplifier input (RINP)
RINN is connected to ground via 1uF capacitor. (J10 engaged when using the EVM)
When the amplifier is powered with <8V I see two problems.
1) The PSRR is very poor below 8V VCC, there is noise on my VCC rail due to the boost converter working in PFM mode. As soon as you go over 7.5V (or there about) the noise disappears.
2) Click/pop is very bad below 8V VCC. Because any change on the AVCC rail is instantly transferred to the internal AVDD/GVDD, so any voltage drop on AVCC when the PWM outputs turn on transfers over to the AVDD and GVDD rails. This creates a pop.
3) In order to improve PSRR due to 1), I placed 50ohm + 10uF RC filter on AVCC. This helps a lot but makes the pop on turn on worse (larger voltage drop on AVCC).
I observe also that when you press the /SD button on the evm, RINP falls to 0v very quickly. Whereas RINN falls very slowly due to the probe resistance.
When you release /SD, RINP rises instantly, RINN takes around 5ms. So it appears that the resistance to Vref for each is different. Therefore when you get any change in Vref (due to change in AVDD, from AVCC), this transfers to an offset in the inputs - causing the pop.
---------------
I believe this is because the internal LDO is set to output 7V so when VCC falls below this, the LDO isn't functioning.
You can repeat my results easily using any codec and the 3136EVM board. Configure it as I have (J13 removed, J10 engaged) then try running the board at 5V then 8V - pressing the shutdown switch on and off.
At 5v the turn on pop is much worse. Also the PSRR is much worse.
Is the AVDD connected to GVDD somehow? Can you show me the internal structure of the power supplies please?
I look forward to your suggestions.
Best regards
David