1. Can the dumped CFG file and .H file show more text description to explain the registers setting.
For example, it can add the specific register name.
2. If tuning 3Watt AGL application, the AGL threshold 1dB adjustment is not convenient
3. Can the GUI generate the .cfg file like the following?
W 54 27 00 00 0C 4A 00 00 18 95 00 00 0C 4A 00 f8 e4 a5 03 86 ea 32
Customer think the following format is not friendly.
.
4. How to adjust the phase, group delay, impulse response and pole zero information for the filter design?