This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS6424 / Efficiency@PVDD=14.4V, Load=4Ω

Hi,

The efficiency @PVDD=14.4V, Load=4Ω is better @2MHz than @384kHz according to Fig 33/34 of the datasheet.

However it is better @384kHz than @2MHz  according to Fig 16/17 of the datasheet.

Which figure is correct?

Best Regards,

Kuramochi