Hi,
TAS5538 can automatically detect the clock error as below.
Could you please tell me the internal behavior during the clock error when halting SCLK and LRCLK ?
An audible noise is heard from the speakers if touching the external components for the pll loop filter when halting only LRCLK.
So, I have some questions as below.
Q1. LRCLK Error
Are the pwm outputs generated by the internal osc clock if halting only LRCLK ?
Or are they generated by MCLK ?
However, MCLK and SCLK are applied to TAS5538.
It seems that they are generated by the internal osc clock.
Q2. SCLK Error
Are the pwm outputs generated by the internal osc clock if halting only SCLK ?
Or are they generated by MCLK ?
MCLK and LRCLK are applied to TAS5538.
It seems that they are generated by MCLK.
Best regards,
Kato