Hi
We have questions of TAS2555EVM and PPC3 as follows.
1. What is difference of ROM MODE1/MODE2 and Tuning mode?
2. PPC3 can generate many configuration files.( xxx_combined_configuration_xx_ROMModexxx.cfg, ...)
How to select which configuration file is used? Do you have explanation of these files?
3. I'm going to evaluate TAS2555 under the following conditions.
-MCLK = 12.288MHz
-Sample Rate = 16KHz
-Bit Resolution = 24bits
Is it possible this evaluation using TAS2555EVM?
Should we update TAS1020B in requested setting?
BestRegards