Hi Sirs,
We are surveying the DRV2700 to support 5uF piezo actuator with 4 ~ 6 pcs in parallel with 200Vpp output, thus the total load capacitance should be around 20uF~30uF. Can we drive those units with single DRV2700 device? There are DRV2700EVM and DRV2700EVM-HV500 options. Which option is ok for 30uF load capacitance?
Thank you and Bets regards,
Wayne Chen
02/20/2017