Hi,
Please help me regarding D-Class AMP_TPA3130D2 pop noise, Please find Attached pdf file.
We designed Audio AMP and use datasheet's reference design on P26 as a post filter
and almost the same connection SDZ FALUTZ as this.
The result is that No POP noise at Power rise but there is another POP noise
at the moment of mute function disabled.
Probably LC rapid and big charging current caused POP noise,( it seems that PWM output is DC,)
Is it possible to make 50% duty PWM output when mute enabled or something else
to reject POP noise?
Regards,