Hi Team,
The datasheet page.23 shows the following and I would like to ask two questions.
1)
What does "interrupt " indicate? Should I regard it as "I2C access"?
2)
I understood there are three options to disable the amplifier as the following.
------------------------------------------------------------------
There are several options to disable the amplifier:
• Write SPK_EN_R = 0 and SPK_EN_L = 0 to the register (0x01, 6 and 0x01, 7). This write disables each speaker amplifier, but leaves all other circuits operating.
• Write SWS = 1 to the register (0x01, 5). This action disables most of the amplifier functions.
• Apply VIL to SDZ. This action shuts down all the circuits and has very low quiescent current consumption. This action resets the registers to its default values.
------------------------------------------------------------------
Is there recommended shutdown sequence for TPA2026D2?
Do you recommend to disable speaker amplifier (SPK_EN_R = 0 and SPK_EN_L = 0 or SWS=1) before applying VIL to SDZ?
Best Regards,
Yaita / Japan disty