Hi Expert,
About TAS5711 0x01 Device ID code. Which one is right? Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jerry,
The initialization value of 0x70 in table 4 should be correct. For table 6 the footnote "(1) Default values are in bold." is not included (unlike tables 5 and 7 where it is included) indicating the value shown is not the default value.
Regards,
Alex
Hi Alex,
Thanks, I will apply TAS5711EVM to read it. Thanks!
BTW, does I saw some E2E record, TAS5711 didn't support 4ohm BTL*2, but my customer is 12V input, does it wupport 5W+5W? or what's the 4ohm output watt suggestion an 12V. Thanks!