Hi Expert,
As title. Or I can add the heat sink to support it? Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jerry,
Actually there exists a good linear relation between the PBTL minimum load impedance and PVCC if you do some simple plotting in Excel. The PBTL minimum load impedance for PVCC@20V should be very close to 1.53ohm based on the equation below.
I would suggest you lower the PVCC to 18V if possible.
Andy