This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM4819: LM4819 Pop noise issue at power down.

Part Number: LM4819

Hi

My customer have the pop noise issue when power down timing.

Output waveforms and schematics are below, 

The condition2 is little bit improved the pop noise than conditon1.  However. customer have to decrease the pop noise more.

Could you please give me your advice for improvement method?

Condition1:  Ci=0.22uF, Ri=47kΩ, Cb=1uF

(Ch1:VDD(5V)  Ch3:Vo2+ Ch4:Vo1-  Math:Ch3-Ch4)

Condition2:  Ci=0.1uF, Ri=100kΩ, Cb=1uF

(Ch1:VDD(5V)  Ch3:Vo2+ Ch4:Vo1-  Math:Ch3-Ch4)

Schematics (same circuit in datasheet)

Thanks

Muk