This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5782MEVM: TAS5782M driver for Windows & Mac ?

Part Number: TAS5782MEVM
Other Parts Discussed in Thread: TAS5782M

Hi TI team,

I have purchased a TAS5782MEVM lately, and bought a PurePath Console Motherboard(AIP006F) a year ago. I had received the access link to my Secure Software last year to download the PPCM3_Version: 3.0.8 for Windows & Mac.

However, After I installed the PPC3_Version 3.0.8 driver, the windows & mac computer both cannot recognize the TAS5782MEVM, and there is no links shown for me to download after I clicked the ( Available EVM Apps ) icon. I can only see "A generic I2C Master for all devices" is only available for download in Windows system, but not shown on Mac.

So For the TAS5782MEVM, do I need other driver for it? where to download? * ( Do you also have the driver for Mac ?  I hope the PPC3+TAS5782M can work on Windows & Mac. )

Thank you

Fai ~