This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5707: About Thermal Parameter

Part Number: TAS5707
Other Parts Discussed in Thread: TAS5733

Hi Sir

Where can I find the thermal parameter of TAS5707 ??

I cannot find it in spec.

thanks for reply.

BR

Yimin

  • Hi Yimin,

    You are looking for thermal metric information such as Junction-to-case or junction-to-ambient thermal resistance, correct?

    Shawn can take a look into this for you and should be posting after the weekend.

    Best,

    Alex
  • Hi Yimin,
    TAS5707 is a very old device, and the way how the thermal data is presented in the data sheet is different from the later devices. The following is the thermal parameters for TAS5707. Hope it helps.
    Theta JA-High K 27.5
    Theta JB 8.9
    Theta JC, bottom 0.9
    Theta JC, top 15.0
    Psi JT 0.3
    Psi JB 8.9
    Best regards,
    Shawn Zheng
  • Hello Yimin! Did this answer your question? Also, have you looked at some of our newer open loop devices like the TAS5733, or event the TAS5751/53? Also, closed loop solutions like the TAS5780 can be of great benefit to optimizing a new solution. Thanks, Jeff