customer reported low resistor issue in pins VO1/2 of LM4670. it looks like EOS issue. is there any comments for for VO1/2 EOS improve?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
customer reported low resistor issue in pins VO1/2 of LM4670. it looks like EOS issue. is there any comments for for VO1/2 EOS improve?
Hi Jose,
This is Jason and Peter is our TI local FAE of LM4670 EOS issue. I would describe my LM4670 failure issue as following.
Since we meet the failure cases frequently in out production line recently, I may need your help to check this issue.
Symptom:
SPK is not functional and LM4670 VO1 (pin5) pin shorted to GND(pin6).
Failure Condition:
both in production line and returned from field
Failure Rate:
16/4230 (2 from field and 14 from production line)
TI FA analysis of first 2 returned defected samples:
LM4670 EOS damage. (see attached FA report from TI)
SPK spec:
3W/4ohm
Questions:
1. I have attached the schematic and layout of my design. Could you help check if any risk of damaging the VO1 or VO2 to short to GND?
2. Has TI been reported similar issue from your other customers?
3. How to avoid the EOS damage of VO1/2?
4. What is the maximum pin voltage endurance of VO1/2 output pins?? the spec seems not to annotate it. I need this data to review if any risks.
5. The FA states the failure is caused by high voltage EOS of VO1 pin, but we can not figure out where the high voltage energy comes from between the defected VO1 and Inductor (EEL21). I don't think the high voltage is from connector side because the varistors (Located after the inductor EEL21 and closed to connector) is NOT damaged. If the high voltage is from connector side, the varistor should be damaged also. I may need your comment on this.
Thanks for your great help.
Hi José,
We input the sine signal into the LM4670 SPK AMP. (CPU outputs the PWM and we use C/R to convert the PWM into sinewave and inputs to SPK AMP)
With your previous reply, we have measure the VO1/2 waveform with and without the output filter inductors.
I found the output overshoot can be as high as 7.2V with output filter INDUCTOR and 6.4V without output filter INDUCTOR .
Could you help check the max voltage overshoot tolerance of LM4670 VO1/2 pins? I can not find any other possibility which can have EOS damage of the VO1/2.
Thanks
Hi Jose,
Could you help clarify if LM4670 is with output short protection? I did an experiment to short VO1 and VO2 when playing sound, the same failure symptom (VO2 short to GND) can be reproduced and the chip is damaged.
I checked the LM4670 datasheet and see it is with short circuit protection, but it seems not with my experiment.
Please help clarify.
Thanks
Jason
Hi Jose,
I am thinking about the necessity of output LC filter or just using the ferrite bead instead.
My application is connecting the SPK AMP to SPEAK by a 1.5M wire harness. I may need your advice about the risk if I remove the LC filter and use ferrite bead instead.
Thanks
Jason,
The change should not generate any problem. Keep in mind a ferrite bead filter is used to reduce very high-frequency interference and LC filter is used for very stringent EMI requirements.
You can refer the Output Filter Desing Considerations to find further information.
Best Regards
José Luis Figueroa
Applications Engineer