Other Parts Discussed in Thread: TPA3116D2, , TPA3118D2, TPA3118D2EVM
Dear Sirs,
My customer asked us about Soft Clip of TAS5760M.
He used TAS5760M & TPA3116D2.
He compared and confirmed the items of Soft Clipper and Plimit in each data sheet.
So the values of Table 4. Soft Clipper Example and Table 3. Power Limit Example were exactly the same.
However, I think that it does not become the same if it is made from measurement formulas.
So question 1
Are both measurement conditions (setting conditions) the same?
Please tell me the conditions of each table.
Also TPA 3116 D 2 has Plimt's characteristic figure on the data sheet but there is no TAS 5760 M soft clip figure.
Do you have it?
Question 2
On the TAS 5760 M data sheet, in describing the SoftClipper function,
There is VP = 4 × VSFT_CLIP.
Is this the clip voltage at no load?
I confirmed with EVM, the Vsft_Clip voltage did not change.
Does the voltage change with or without load?
Best Regards,
Y.Hasebe