This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5782M: performance compared with TAS5756M

Part Number: TAS5782M
Other Parts Discussed in Thread: TAS5756M, TAS5756MDCAEVM,

Hello

In same condition which is PVDD=12V 8ohm 1W, THD+N is different as following.

;TAS5782M  0.014%

;TAS5756M  0.007%

Is it due to difference of internal DAC performance ?

( Customer think so, but is it correct?

In regard to idle channel noise, both  TAS5782M and TAS5756M is almost same...

Is data sheet correct?)

Best Regards