Hi,
When I am using LM4950 audio amplifier with a 12V/2A adapter, it works completely fine, but when I connect to a 12V battery (can source up to 20 A current) the amplifier burns. I tested it with two boards and got the same result. The DAC_SHUTDOWN pin is floating in the beginnig. The output of the amplifier is connected to the transformer and no load is connected to the output of the transformer.
Any ideas?
Regards