Other Parts Discussed in Thread: TAS5754M
Hi,
The junction temperature for the digital and power die is mentioned on page 9 of TAS5782M datasheet, the over temperature error is also mentioned on page 12.
I am concerned that it will affect the digital die when the junction temperature on the power die rises because the digital die and the power die are adjacently placed in the package.
So, is there a possibility that the junction temperature will rise more than 125℃ on the digital die and the malfunction will be caused when detecting the over temperature error(more than 165℃) on the power die ?
Best regards,
Kato