Good morning
One of my clients is using the TAS5782M for this project.
Can you review it?
I will send you the corresponding schematic file.
<<schematic deleted>>
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello! Andy will take a look at your schematic, but you should also pay careful attention to the Layout. The attached relates to an automotive part, but the guidelines are important to any design. Thanks, JeffTAS6424 Layout Guidelines for EMI.docx
Sorry for my late response.
See my comments below.
a) C5, C6, C7 and C8
Our recommendation is ceramic, 22uF, ±20%, X5R. The voltage rating must be > 1.45 * PVDD.
b) C20, C21, C23, C24
Our recommendation is ceramic, 2.2uF, ±10%, X5R. At a minimum, voltage rating must be > 10V.
c) C22
Our recommendation is ceramic, 1 μF, 6.3V, ±10%, X5R.
Andy