Other Parts Discussed in Thread: TPA3245, LM5010
Hi,
I'm designing an audio power amplifier using TPA3221. have pretty limited space for my board so I'm looking at minimizing the footprint for the output filter.
The inductor 10uH) and cap (1uF) that are used on the EVM-board are bigger than I can fit!
I wonder if it is possible to use alternative more compact inductors and capacitors!
I have been looking at this inductor:
ETQP4M100KVC from Panasonic
ETQP4M100KVC (output filter inductance 10uH).pdf
Regarding the caps I have not found any yet! Could someone recommend me a smaller cap that could work well! Smaller than the one on the TPA3221-EVM!
Best regards
Markus