Other Parts Discussed in Thread: TPA6211A1, PCM5100
Hello,
My customer has a pop noise problem with TPA6211A1 during 5V power up. The background and tests we have done are listed as the following.
1. Input of TPA6211A1 is single ended and IN- is coupled with PCM5100 with 1uF capacitor and IN+ is connected to ground with 1uF and 20K resistor in series.
2. /SD is alway keep low after 5V start-up.
3. when 5V power is off and turned on after a short within a few sends, we will hear the pop noise, enven the /SD is still low.
4. We do see an unballanced output during 5V power-up and unballanced input.
My questions is that: the output of TPA6211A1 should be high impedance when /SD is pulled low, why there is unballaced output, especially when Vcc exceeds 2.5V? Is there anyway to avoid the pop noise?
Below is the waveform we captured.