Hi
1.
According to datahseet, the junction temperature is limited by 150℃ but thermal protection works at 165℃.
What is relationship between thermal protection and absolute junction temperature?
2.
Are there any impact for device performance if device works between 165℃ to 155℃?
3.
The "typical" electrical characteristics would be offerd in Ta=25℃.
What is temperature in "limit" characteristics?
4.
What is Tc (case temperature) when thermal protection works?
Do you have information?
BestRegards