Hi Audio Folks,
One of our customer used the LM48511, and found the device is easy damaged. and the output power is 4W when the load is about 4ohm. Power supply is 4.5V. and we also measured the boost voltage is about 7.2V.
the customer tested about 30pcs and do warm experiment test about 24 hours. and found there were 3-5 pcs damaged. and we also do the FA test. here is the test report.
so, it shows it has EOS damaged in Pin 8 and Pin12 . and the Pin 8 and Pin12 are the output pins.so the customer wonder to know how it cause this problem. by over-temperature or over-voltage? because the customer want to avoid this issue before mass production.
so do you have and comments for this issues? or is there anything else we need to be noticed? it's really urgent for us now. Thanks in advance.