Hi,
I would like you to confirm about below.
*
Now, customer consider how much current will be required when speaker is active.
They have information about speaker load and supply voltage which they will use. so I think that I can estimate approximate current from figure 13.
However, I'm not sure efficient in case of above.
So, the question is
* Is it the way to estimate approximate current from above figure ?
(One of example, they will use 2 ohm load, 14.4V PVDD and Fin 1kHz, then available power is arround 50W. However I'm not sure efficient in this case so I could not calculate by using "P=V^2/Rload")
Thanks in advance,
Machida