Hi,
We developed the boards with TPA6211A1-Q1. We are sending an audio pulse with different harmonics as an input for "single ended input application". Gain is set to 1.72. Input signal is 600mV pk-pk with 1.545V max and 0.956V min. A 4ohm speaker is being driven and IC's Vcc is 2.8V.
Problem is: When the audio in signal is sent, we see a high power consumption by audio IC for few milliseconds. Is that expected? or do we need something to take care. Currently my application a low power application so power consumption spike is not accepted.
Regards,