Other Parts Discussed in Thread: TAS5766M, TAS5756M
When I play ~800 hz sinus test data on TAS5768M (I2S bus used) after some %60 value of the volume, output of the TAS5768M deteriorates
actually voltage over cutted from above and bottom , I used Pure path console and only and register dump to h file then load to the TAS5768
chip, I don't use any EVM for this work, can you help please?
used platform :PPC3 console
ı2s bus 44100 hz ,16 bit data
target voltage 12V
is there any way like AGC (aoutomatic gain control) for solving that problem