Hi,
I worked with the TPA3116D2 and tried BTL and PBTL, but it was always stuck in the fault/protected state (faultz = low).
The basic circuitry is as seen below
Sync was left floating
SD=5V
Mute=GND
Output plug open
Measurements:
GVDD=6.9V
PLIMIT=6.9V
FAULTZ=0.1V
RINP/N=2.8V directly on the pins
PVDD is either 12.5V or 25V, but the results remained the same. Also tried ferrite beads and 1nF caps instead of the 10uH coils with 1uF caps or leaving the secondary site open (just bootstrap caps).
This exact behaviour was seen on multiple boards.
Regards,
Dominik