Hi,
I would like to know about absolute ratings of parts for LC filter.
About L(10uH);
For example, The circuit of Figure 50 in datasheet page 30, VDD=30V, 4ohms Speaker
In this case, Should we use the inductor which accept over 7.5A(=30V/4ohms)?
Or Can we use the inductor which accept under 7.5A(This is by calculated current value at max gain output of using case)?
About C(1uF);
For example, The circuit of Figure 50 in datasheet page 30, VDD=30V, 4ohms Speaker.
In this case, How much voltage capacitor as breakdown voltage should we select?
Best regards,
Shimizu