This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5614: Need TC Specification of TAS5534 and TAS5614

Part Number: TAS5614

Hi Sirs,

Would you pls advise the Tc temperature specifications of the TAS5534 and TAS5614 devices per customer's request?

Thank you and Best regards,

Wayne Chen
08/16/2018

  • Wayne,

    Are you requesting the thermal numbers as below? 


    Regards,

    -Adam

  • Hello Adam,

    Thanks for your concern. Customer needs the Tcase (case temperature) spec, not thermal resistance. The TAS datasheet provides  Tj (junction temperature) and Rjc (junction to case thermal resistance) specifications, thus product line should have official Tcase specification. Customer can measure the Tcase temperature, so we need product line's official data to judge customer's test result.

    Thank you and Best regards,

    Wayne Chen
    09/06/2018

  • Wayne,

    This is not something we measure or specify because it is highly dependent on many factors.

    This varies according to heatsink, IC mounting, solder profile, heatsink compound, heatsink attachment, heatsink material, etc...

    Regards,

    -Adam


    If your question was answered, please click the "This resolved my issue" button!