TAS5615 Response Outside Audio Range

Q: TAS5615

Hello,

My input frequency can range from 5-50 kHz. I am curious as to what kind of attenuation I could expect from the TAS5615 from 20-50kHz.

Thanks.


A: Re: TAS5615

Hi,

The 5615 should be flat up to 80kHz input frequency. Obviously you might need to change the output filter a little bit, but the amplifier itself should work at 50kHz input perfectly fine.