Q: Does TPA3124 support 3ohm load?  

Is there any performance data of the TPA3124 for the following condition:

Output power=stereo 5W, load=3ohm, PVCC=12V, SE mode.

 
A: RE: Does TPA3124 support 3ohm load?

Here is the performance for 3 ohm load at 12V PVDD.

2350.TPA3124 Output Power THD.pdf

Note: 3 ohm load is only supported in single ended mode.