Welcome to the Audio Amplifiers Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".
Q: TAS5707 and TAS5602 Idle current by
Hello,
Could you let us know following data of TAS5707 and TAS5602;
-Quiescent supply current at Condition 1: Idle (no output), PVDD = 16V, RLoad = 4ohm Condition 1: Idle (no output), PVDD = 16V, RLoad = 8ohm
A: RE: TAS5707 and TAS5602 Idle current
Data measured on EVM:
For the TAS5707 I measured the following current coming from PVDD:
4 ohms: .117A
8 ohms: .116A
Note that this does not include the current going into DVDD which is about 48mA.
For the TAS5602,
4 ohms: .06A
8 ohms: .059A
In both devices, there is almost no change in currents because the output filters are able to block most of the switching frequencies. As Don mentioned earlier, a different filter might cause much higher currents.