Q: TPA6017A2 gain inputs not defined in datasheet

The datasheet for the TPA6017A2 does not electrically specify the VIH/VIL levels for the  gain inputs.  Please specify. 


A: Re: TPA6017A2 gain inputs not defined in datasheet

Recommended operating conditions:

VIH: Min = 0.8 * VDD

VIL: Max = 0.4*VDD

If these levels are applied to the gain pins the device will work as expected.