This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA226: How to sense motor current with INA226 in a H-bridge (VNH2SP30)?

Part Number: INA226

Hi,

I am actually using a Hall Effect based current sensor (ACS714) inline between to the Motor in the H-bridge.

My V+ is 5.5V, the H-bridge is a VNH2SP30 based evaluation Board (Sparkfun MonsterMoto-Shield).

Since the internal current sensor from the VNH2SP30 is not accurate enough and the Hall Effect based one gets massive electromagnetic distortions from the turning motor, I wanted to evaluate the INA226 as a replacement.

What is the best way of current measuring? Can I simply replace the ACS714 with an INA226 and a proper shunt or do I have to switch to low-side current sense?

Thank you,
Alex

1 Reply

  • Hi Alex,
    Thank you for posting on the E2E Forums.

    You can use the INA226, but accuracy will be affected by common mode swings if you are using PWM to drive the motor.
    I suggest a look into the INA240 as a better replacement option due to the better common mode rejection. You can set an analogue reference at 1/2VCC (2.5V?) and have a drop in replacement for your hall sensor.

    As to the electromagnetic distortions... are you differentiating the freewheeling currents by synchronizing the ADC readings with the PWM on time? If not you will get opposite readings during the PWM off time.

    Kind Regards,

    Carlos S.

    TI makes no warranties and assumes no liability for applications assistance or customer product design. You are fully responsible for all design decisions and engineering with regard to your products, including decisions relating to application of TI products. By providing technical information, TI does not intend to offer or provide engineering services or advice concerning your designs.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.