I had a question about the INA168(Current Shunt Monitor). I have Rs=0.1ohms(0.1%), RL=50k(0.1%), and the Is(the current across Rs) should be very close to 0A when measured with a multimeter. For some reason, I keep getting a voltage of 0.4V on RL, which would mean that my current(Is) is 0.4A. Am I thinking of the math incorrectly?